InfoPlatform Service Installation Package

NOTE:
Ensure that the following packages are installed before installing InfoPlatform.
The install file is named with the following format:
  • Download the FactoryTalk Analytics InfoPlatform Service.M.m.r.bbbb.msi
    Where M.m.r.bbbb is the version number of the service:
    • M: major
    • m: minor
    • r: revision
    • bbbb: build number
    IMPORTANT:
    To install FactoryTalk Live Data, install “FactoryTalk Service Platform” as needed.
FactoryTalk Analytics InfoPlatform Service depends on a number of other software products whose installation media are not included with this product. The paragraphs below identify these products and their installation media. Prior to installation, check if they are already present on the target system. Unless otherwise indicated, the following can be found on the installation media for FTHistorian at the locations indicated.
NOTE:
Names and exact locations may differ depending on the version of FTHistorian being used.
NOTE:
If FTServicePlatform is already installed, user must apply the FTSP patch. Refer to KB RAID 1092336:
https://rockwellautomation.custhelp.com/app/answers/detail/a_id/1092336
  • FactoryTalk Service Platform, FactoryTalk Directory (Note: FTDirectory may be installed on a separate computer)
    Redist\6.00.00-FTServices\setup.exe
  • OSI PI SDK
    Redist\PISDK\setup.exe
  • OSI AFClient
    Redist\Enterprise\AFClient_x64.msi
  • OSI PI System Management Tools
    Redist\PISMTSetup\PISMT3.msi
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal