Create a product inventory report
To create a product inventory report
- On theProduct Inventory & Registrationtab, on theNew Inventorypage, clickName Inventory.
- In theInventory Namedialog, enter the inventory name, and then clickGo to Select Path.
- In theNetwork Browserdialog box, select a node, select the level from theChoose number of levels to browselist, and then clickOK. The devices list is generated differently depending on what is chosen as the starting node. See Generating the devices list for the detailed information.
- After the browsing is completed, selectView full inventoryto see the CSV file, selectBackto start another inventory, or selectSend Inventoryto send the inventory report to your Rockwell Automation account.TIP:If the inventory only contains one device, the starting point for the browse may have been a device instead of a driver, network, or backplane.
Provide Feedback