Flash multiple devices concurrently
After the firmware revisions on the Product Compatibility and Download Center are downloaded, you can start to flash the selected devices.
TIP:
When you are flashing FLEXHA 5000™, we recommend that you avoid flashing the adapter and
IO concurrently. Make sure you are using a path to the IO that doesn't go through the
adapter that is being updated.
To flash multiple devices concurrently
- On theFlash Devicestab, confirm the devices and revisions, and then selectNext.
- Read and understand all warning messages shown before proceeding.
- SelectFlash.TIP:When a dialog box prompts you to confirm whether to trust the publisher of a DMK during the update, you can choose to trust it to continue.Flash Resultsprompts. check the flash results, and then close it.
- SelectDone.If you want to view the flash report, selectDoneafter you open the Reports folder.
Provide Feedback