Channel X - Modbus Slave view parameters
Use the
Channel
view to define the characteristics of the Modbus Slave.X
- Modbus SlaveThe
Channel
view includes these parameters:X
- Modbus SlaveParameter | Description |
|---|---|
Modbus Format | Determines whether the Modbus transmission format is Modbus RTU or Modbus ASCII .The default is Modbus RTU. |
Inter-Frame Timeout | Specifies maximum delay time to receive data for the Remote Terminal Unit (RTU). Tip: This parameter is available only when Modbus Format is set to Modbus RTU . |
Node Address | Specifies the node address of the slave. Valid value is from 1 through 255. The default is 1. |
Diagnostics | When online, opens the diagnostics dialog box to view diagnostic counters for performance and error management with the Modbus Slave. |
Provide Feedback