Channel X - Modbus Slave view

Use the
Channel
X
- Modbus Slave
view to configure the Modbus Slave.
Use the
Channel
X
- Modbus Slave
view to:
  • Select whether the Modbus transmission format is
    Modbus RTU
    or
    Modbus ASCII
    .
  • Enter the
    Inter-Frame Timeout
    for the
    Modbus RTU
    .
  • Enter the
    Node Address
    of the slave device.
  • Open the diagnostic dialog box to diagnose a communication problem with the Modbus Slave.
The
Modbus Slave
view is available when
Channel
X
in the
Device definition
dialog box is set to
Modbus Slave
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal