Channel X - Modbus Master view
Use the
Channel
view to configure the Modbus Master:X
- Modbus Master- Select whether the Modbus transmission format isModbus RTUorModbus ASCII.
- Define theResponse Timer.
- Enter the delay after the data broadcast.
- Enter the maximum number of times to retry the request.
- Enter theInter-Frame TimeoutforModbus RTU.
- Open the diagnostic dialog box to diagnose a communication problem with the Modbus Master.
The
Modbus Master
view is available when Channel
in the X
Device definition
dialog box is set to Modbus Master
.Provide Feedback