Channel X - Generic ASCII Transmit view parameters
Use the
Channel
view to configure the Generic ASCII Transmit mode.X
- Generic ASCII Transmit The
Channel
view includes these parameters:X
- Generic ASCII Transmit Parameter | Description |
|---|---|
Swap Mode | Determines how the data transmitted to the serial port is arranged. The swapping is done before the device sends output data. Available options are:
|
Termination Mode | Determines the usage of the termination delimiters in the data. Available options are:
Tip: The termination delimiter is only applied when Ox.ASCII.TXDataLength = 0. |
Termination Delimiter 1 | Specifies the channel's first termination delimiter. The termination delimiter is used to signal the end of the data. Valid values are:
|
Termination Delimiter 2 | Specifies the channel's second termination delimiter. Valid values are:
Tip: To use only the first termination delimiter to signal the end of the data, set the Termination Delimiter 2 to $FF . |
Diagnostics | When online, opens the diagnostics dialog box to view diagnostic counters for performance and error management with the Generic ASCII Receive/Transmit communication. |
Provide Feedback