Channel X - Generic ASCII Transmit view
Use the
Channel
view to define the data transmitted to the serial device:X
Generic ASCII Transmit- Select the swapping mode for data transmitted to the serial port.
- Select the termination mode.
- Specify the termination delimiters.
- Open the diagnostic dialog box to diagnose a communication problem with the Generic ASCII Receive /Transmit communication.
The
Generic ASCII Transmit
view is available when Channel
in the X
Device definition
dialog box is set to Generic ASCII
.Provide Feedback