Calibration Wizard parameters

The
Calibration Wizard
includes these parameters:
Parameter
Description
Channel
Displays the channel number to which this configuration applies.
Calibrate
Identifies the channels for calibration.
Select the check box that corresponds to the channel number you want to calibrate.
Calibration Range
Displays the value currently configured for the channel. Values display according to the Input Type selected.
Calibration Gain
Displays the calibration gain values as reported by the module.
Calibration Offset
Displays the offset in signal units as reported by the device.
Calibration Status
Displays the status of the calibration per channel as the calibration occurs.
Calibrate Channels in Groups
Select this check box if you want to calibrate multiple channels as a group.
Calibrate Channels One at a Time
Select this check box to calibrate one channel at a time.
Low Reference
Displays the value of the low reference signal for the channel.
High Reference
Displays the value of the high reference signal for the channel.
Recorded Reference
Indicates the measured output values.
Low Recorded
Displays the recorded low reference value in signal units.
High Recorded
Displays the recorded high reference value in signal units .
Status
Displays the value read during calibration for the enabled channels.
  • OK - Indicates that the reference signal is within the acceptable range.
  • Error - Indicates that the reference signal is not within the acceptable range
If Status shows Error, measure and enter the recorded reference values again for the channels in error, and then select Retry.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal