Calibration Wizard parameters
The
Calibration Wizard
includes these parameters:Parameter | Description |
|---|---|
Channel | Displays the channel number to which this configuration applies. |
Calibrate | Identifies the channels for calibration. Select the check box that corresponds to the channel number you want to
calibrate. |
Calibration Range | Displays the value currently configured for the channel. Values display according
to the Input Type selected. |
Calibration Gain | Displays the calibration gain values as reported by the module. |
Calibration Offset | Displays the offset in signal units as reported by the device. |
Calibration Status | Displays the status of the calibration per channel as the calibration occurs. |
Calibrate Channels in Groups | Select this check box if you want to calibrate multiple channels as a group. |
Calibrate Channels One at a Time | Select this check box to calibrate one channel at a time. |
Low Reference | Displays the value of the low reference signal for the channel. |
High Reference | Displays the value of the high reference signal for the channel. |
Status | Displays the value read during calibration for the enabled channels.
If Status shows Error, investigate the channels with errors, and then select
Retry. |
Provide Feedback