Calibration Wizard view (Input Modules)
Use this wizard to calibrate the analog modules. To perform the calibration process, the
module must be inhibited or online with the controller in Program Mode.
When you calibrate input modules, use current, voltage, or Ohms calibrators to send a
signal to the module to calibrate it.
These options are available in the Calibration Wizard:
- Calibrate Channels in Groups:TIP: Use this option to apply a reference signal to all of the selected channels at the same time.
- Enter calibration mode.
- Attach low reference signals to all selected channels.
- Sample all of the selected channels.
- Attach high reference signal to all of selected channels.
- Sample all of the selected channels.
- Complete the calibration.
- Calibrate Channels One at a Time:TIP: Use this option to apply a reference signal to the selected channels one-at-a-time, and then move on to the next channel.
- Enter calibration mode.
- For the first selected channel, attach low reference signal.
- Sample the first selected channel.
- For the first selected channel, attach high reference signal.
- Sample the first selected channel.
- Complete the calibration for the first selected channel.
- Repeat the above steps for the remaining selected channels.
Provide Feedback