Port Configuration view parameters
Port Configuration
view includes these parameters:
TIP:
These parameters are available when the project is
online.
Parameter | Description |
Refresh | Retrieves and displays the latest information from the device. |
Set | Writes pending edits to the device.
TIP:
|
Ethernet | |
Port | Displays the port number. |
Enable | Select or clear the checkbox to enable or disable the port. |
Link Status | Displays the status of the port communication on the network. |
Auto-Negotiate | Indicates that the device automatically selects the best method for
communication. If cleared, the port speed and duplex must be set manually. |
Speed – Selected | Specifies the configured port speed for sending and receiving data. Available
options are device dependent.
TIP:
Selected
Speed is unavailable if Auto-Negotiate is selected.
|
Speed – Current | Displays the actual speed at which the port is currently sending and receiving
data. |
Duplex – Selected | Specifies the configured port duplex setting:
TIP:
Selected Duplex is unavailable if
Auto-Negotiate is selected.
|
Duplex – Current | Displays the actual duplex method that the port is currently using to send and
receive data. |
Port Diagnostics | Opens the Port Diagnostics dialog to view the interface and media counters for
the port. |
NFC | |
Enable Near Field Communication (NFC) | When selected, NFC is enabled. You can disable NFC by clearing the
checkbox. |
Provide Feedback