Port Configuration view

Use
Port Configuration
to view and configure the port settings. The settings define how data is sent and received between the port and the attached device. The
Port Configuration
view is only available for devices with an embedded Ethernet port, and the configured values are only displayed when the device is online.
IMPORTANT:
Configuring the port settings involves writing data to the device, which interrupts the connection to the controller and to any other device that is connected through it. Connections from other controllers may be interrupted as well. Ensure a connection interruption at this time is acceptable before proceeding.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal