IO-Link (Generic) parameters

The IO-Link (Generic) parameters apply to the following channel mode types:
  • IO-Link (Generic), Input Output, Timestamp
  • IO-Link (Generic), Input Output
The IO-Link (Generic) parameters include:
Parameter
Description
IO-Link port event log
Opens the XX – IO-Link Port Event Log dialog to view diagnostic information.
Disable and delete Data Storage
Disables Data Storage and deletes the master copy of the Data Storage on this port.
Enable Data Storage if supported
Enables Data Storage for the attached IO-Link device.
Validate device identity
Validate the identity of the attached IO-Link device.
Vendor ID
The expected vendor ID of the attached IO-Link device to validate.
Device ID
The expected device ID of the attached IO-Link device to validate.
IO-Link Revision
The expected IO-Link revision number of the attached IO-Link device to validate.
IO-Link device event log
Opens the XX – IO-Link Device Event Log dialog to view diagnostic information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal