XX – IO-Link Device Event Log dialog
The
IO-Link Device Event Log
dialog displays the reported events that are stored
in the event log of the IO-Link device. Use this dialog to:- View the event log.
- Refresh the data on the screen.
- Clear the event log.
Provide Feedback