XX – IO-Link Device Event Log dialog parameters
Parameter | Description |
|---|---|
Timestamp | Displays the timestamp of the event that occurred. The format is
YYYY -MM -DD -HH :MM :SS :SSS . |
Type | Displays the type of event received from the IO-Link device. Possible values
are:
|
Mode | Displays the mode of the event received from the IO-Link device. Possible values
are:
|
Description | Displays the description of the event based on the Event Code. |
Event Code | Displays the code for the event received from the IO-Link device. The format is
0x HHHH . |
Refresh | Updates the event log for this port. |
Clear log | Clears the event log for this port. |
Provide Feedback