Input EventXX view parameters

Parameter
Description
Enable event
Determines the corresponding event trigger definition to activate. Events are triggered once when conditions match the definition.
Latch event
Determines whether an event is latched until it is acknowledged.
Enable independent point triggers
Determines whether each condition indicated in the Event trigger definition can initiate an event independently.
Trigger event
Triggers an event each time an input state change results in conditions:
  • matching the event trigger definition, or
  • no longer matching the event trigger definition.
Participate in Event Trigger
Determines whether the specified point participates in the Event trigger definition for the event.
State Transition
Determines the state of the input after the transition.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal