Input EventXX view

Use the
Input EventXX
view to view the device at the individual event level.
TIP:
The
Input EventXX
view is available only when
Connection
in the
Device Definition
dialog is set to one of these values:
  • Data with Events
  • Data with Events and Status
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal