Input Events view parameters
Parameter | Description |
|---|---|
Event | Indicates the event number to which this configuration applies. |
Enable Event | Shows whether the corresponding event trigger is active. Events are triggered once
conditions match the event definition. |
Latch Event | Shows what happens to the current event when a new event is received. |
Provide Feedback