Input Events view
Use the
Input Events
view to:- View a summary of the events configured for the device.
- Access theInput Event0Xview to view parameters for a specific event.
TIP:
The
Input Events
view is available only when Connection
in
the Device Definition
dialog is set to one of these values:- Data with Events
- Data with Events and Status
Provide Feedback