Device Information view

Use the
Device Information
view to display device and status information when the device is online.
Use the
Device Information
view to:
  • Determine the identity of the device.
  • View the device's current operational state.
  • View whether the device is configured by the owner controller.
  • View whether an owner controller is currently connected to the device.
  • Retrieve the latest information from the device.
  • Reset a device to its power-up state.
TIP:
The data in the
Device Information
view comes directly from the device. The
Device Information
view is not available when the communication format is Listen-Only.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal