Device definition dialog box parameters
Parameter | Description |
|---|---|
Device type | Displays the type of the device being configured. |
Name | Specifies an IEC 61131 compliant device name. The name must be a unique name without any invalid characters. |
Description | Specifies the device description. |
Ethernet address | Specifies the IP configuration for the device. Possible options include:
|
Enable Network Address Translation (NAT) | Enables the safety communications to a device addressed through NAT. |
Actual device address | Specifies the device's IP address on the Private Network of the NAT. It is the same IP address found in the Internet Protocol view.This parameter is available when the Enable Network Address Translation (NAT) checkbox is selected. |
Revision | Specifies the major and minor device firmware revision level. The major revision indicates the revision of the interface to the device. Valid values are from 1 through 127. The minor revision indicates the firmware revision. Valid values are from 1 through 255. The default is 1. |
Electronic keying | Reduces the possibility of using the wrong device in a control system. The valid values are:
|
Input status | Determines the type of input status for the device. See Input data status and description for more details. |
Input data | Determines the type of input connection for the device. See Input data status and description for more details. |
Output data | Determines the type of output connection for the device. Valid values include:
|
Data format | Determines the format of data exchanged between the parent and the device. |
Provide Feedback