Device Information view
Use the
Device Information
view to view device and status information when the device is online.Use the
Device Information
view to:- Determine the identity of the device.
- View the device's current operational state.
- View whether the device was configured by the owner controller.
- View whether an owner controller is currently connected to the device.
- Retrieve the latest information from the device.
- Reset a device to its power-up state.
- If supported, view the protection mode of the device.
- If supported, clear current faults of the device.
- If supported, configure the system status indicator for device identification.
TIP:
The data in the
Device Information
view comes directly from the device. The Device Information
view might not be available when the connection is set to Listen Only.Provide Feedback