HART Device Inhibiting
You can suspend data exchange between the controller and individual HART devices, either
in offline mode (applies after download) or online mode. Inhibition does not make the
device cease operation. This option allows for maintenance of the device without faults
being reported to the controller.
You can inhibit HART devices on the Connection view of the Properties window for the HART
device.
Provide Feedback