HART Bus
Every HART device is added as a CIP node on the HART bus that is
associated with the HART I/O module.

You can use the HART bus in the I/O Configuration tree to:
- Add or remove a HART device.
- See the warning or inhibit status icon of an attached HART device.
- Open the properties for the HART device.
Provide Feedback