Execute HART Commands Through Explicit Messaging
PointMax analog HART I/O modules allow you to define message instructions to send
commands to HART devices. The CIP service is Service 0x4C of HART Process Device Object
that is defined in CIP Volume 7B “Integration of HART Devices into the CIP Architecture”
with an exception that Class ID 0x3B8 should be used for HART Process Device Object.
As executing HART commands through explicit messaging causes delays of updating dynamic
or device variables in the producer data of the HART device, periodical command
execution through explicit messaging, for example, connected and cached message
instruction, is not recommended.
Provide Feedback