Reset IO-Link Device to Factory Default
When you reset an IO-Link device to factory default, all parameters are reset to their
default values.
To reset an IO-Link device to factory default, complete these steps.
- In the IO-Link device Module Properties → Device Information view, select Reset Module to Factory Default.
- Select Apply.
Provide Feedback