IO-Link Device Applications
This chapter describes how to add and configure IO-Link devices that are connected to
your IO-Link master module in a Studio 5000 Logix Designer application project.
You must complete the following tasks before you can configure the IO-Link device:
- Create a Studio 5000 Logix Designer application project.
- Add a controller to the project.
- Add and configure an IO-Link master module.For more information, see Add a New Module to a Studio 5000 Logix Designer Application Project.
- Set at least one channel mode to one of the following:
- IO-Link
- Digital Input, Fallback
- Digital Input, Timestamp, Fallback
Before using the IO-Link capabilities, verify the following:
- The IO-Link master module and any associated field devices are working properly.
- The field device is IO-Link capable.
- Only one IO-Link device is connected to each port.
- The IO-Link master module has established connection with the controller at least once after the module has cycled power or has been reset.
Provide Feedback