Construct a PointMax I/O System
The PointMax I/O system contains the components pictured below.
PointMax I/O System
Item | Component Name | Description |
|---|---|---|
Adapter | The adapter transfers data between the I/O module and the
controller. | |
Removable Terminal Block (RTB) | The RTB contain terminals to terminate wiring for field devices.
Also it has interfaces to establish the connection between the
RTB and the I/O module. | |
I/O module | The I/O module contains the Sensor Actuator (SA) or field power
interface and circuitry needed to perform specific functions
related to your application. | |
Mounting Base (MB) | The MB contains mechanical and electrical interfaces to establish
the connection between I/O module and the backplane. | |
End cap | It is a dust protection cap for the last module in a rack. |
For PointMax I/O system power requirements, see PointMax I/O System Installation
Instructions, publication 5034-IN001.
IMPORTANT:
Confirm that SA power is connected for proper operation of safety I/O modules.
Provide Feedback