Delete a data set
Data sets are components of a data log. A data log records the data values of a defined set of variables in a controller project.
Prerequisites
- The project is offline.
To delete a data set
- In theControllertree, selectData log.
- On theData Logconfiguration page, from the data log list, clear theDSET<x>checkbox.
- InDelete variables, selectDelete.
Provide Feedback