Open the variable selector from controller configuration pages
Open the variable selector to navigate between variables of different scopes and add variables for the following
Micro800
configurations:- Modbus mapping
- MicroLogix mapping
- DNP3 mapping
- Data log
- Recipe
By default, opening the variable selector from a
Micro800
controller configuration page displays the global variables in the project.Prerequisites
To open the variable selector from controller configuration pages
- InProject Organizer, double-click the controller node.
- From the controller tree, select one of the following:
- Modbus Mapping
- MicroLogix Mapping
- DNP3 Mapping
- Data Log
- Recipe
- On the configuration page, do one of the following:
- In the empty row, double-clickSelect variable.
- In the empty row, select
.
Provide Feedback