Add a controller to the project
Use
Add device
to add a controller to a FactoryTalk Design Workbench
project. FactoryTalk Design Workbench
supports one controller for each project.After selecting a controller, in the
Selection
pane of the Add device
dialog, the following controller information is shown:For more information about devices, see Controllers catalog.
Prerequisites
- Create a project without adding a controller.
To add a device to a project
- OpenAdd deviceby doing one of the following:
- InProject Organizer, right-click a blank space, and then selectNew device.
- InProject Organizer, select theNew devicebutton.
- InAdd device, double-click the controller you want to add or select the checkbox beside the controller.
- InSelection, enter the controller name, select the controller revision, view the controller lifecycle information, and then selectAdd.
Provide Feedback