Delete a plug-in module from the controller
Deleting a plug-in module removes the input and output variables from the controller configuration.
After deleting a plug-in module, update the Project Organization Units, interrupt definitions, Modbus address mappings, MicroLogix mappings, and DNP3 mappings that use the input and output variables of the plug-in module.
To delete a plug-in module from the controller
- InProject Organizer, go to .
- UnderPlug-in, right-click the module, and then selectDelete.
After deleting a plug-in module, the slot numbers of other plug-in modules remain unchanged.
Provide Feedback