Cabinet Mount the Supplemental Power Tap
- Place the power tap against the mounting surface.
- Check for level, then place a mark at each mounting hole location
.
Supplemental Power Tap Mount in Cabinet (shown with 1486-CON connectors attached) - Drill holes at the marked locations.
- Align the power tap to the mounting holes, the secure them with two M4 or #8 screws and washers.
Provide Feedback