Local library and template file
By default library object files and template files are stored in this location:
C:\Users\Public\Documents\Studio 5000
There are separate subfolder in each. The library object repositories,
Libraries
and Templates
folders with an Application Code Manager
(RA-LIB) ACM 2.00
and (RA-LIB) Process
, and the template repository, (RA-TPL) ACM 2.00
, are in their respective subfolders.The
(RA-TPL) ACM 2.00
folder is set as the default documentation path for the Application Code Manager
application. To change the documentation path open ACM Default Settings and specify the path to use.In
C:\Users\Public\Documents\Studio 5000\Samples\Application Code Manager\Example
,
you can find the Area Model sample file.
TIP:
If working in a collaborative design environment with a shared ACM database, template files can be copied to a shared folder so that all users can access them.
Provide Feedback