Title bar

RSLinx Classic Linked Icons PNG FIle Template
The title bar contains the RSLinx Classic icon, the name of the software product (for example, Rockwell Software RSLinx Classic Gateway), the RSWho instance number (RSWho - 1 opens by default when you open RSLinx Classic), and the Minimize, Maximize, and Close button.
You can also click the RSLinx Classic icon to display the Control menu in the title bar.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal