Control menu

To access the
Control Menu
, click the RSLinx Classic icon RSLinx Classic Linked Icons PNG FIle Template at the top left portion of the screen. The
Control Menu
contains the following items:
  • Restore
    returns the window to its former size before it was enlarged (using the Maximize command) or shrunk to an icon (using the Minimize command).
  • Move
    allows you to use the keyboard to move the window to another position on the desktop.
  • Size
    allows you to use the keyboard to change the size of the window.
  • Minimize
    shrinks the window to an icon.
  • Maximize
    enlarges the window to its maximum size.
  • Close
    terminates the application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal