Data table monitor

How do I access the data table monitor?
In the
RSWho
, right-click a controller, and select
Data Monitor
from the context menu.
Use RSLinx Classic data table monitor to view ControlLogix, PLC-5, SLC, and MicroLogix data. You can open a separate data table monitor for as many processors as needed. This procedure is called data monitoring. When you are monitoring your data, the information displays in either a data file list window or a data table window. Data monitoring allows you to:
  • Select data files to be viewed
  • View the data files in a grid format
    IMPORTANT:
    • The data table monitor is read-only. Values in the data files cannot be modified directly from the data monitor window. However, for PLC-5 and SLC controllers, elements can be copied to the clipboard and be read or written with DDE. Input and Output files are protected against writes with DDE.
    • For ControlLogix controllers, if you set the tags to read-only, values in the data files cannot be modified from neither the data monitor window nor the DDE.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal