Edit an existing name or phone number
How do I access this dialog box?
To access the
Dialer Configuration
window, refer to the Configure a modem dialer help topic.- From theDialer Configurationdialog box, expand the phone book and select the name or phone number you want to edit.
- SelectEdit > Modify.
- In theEdit Phone Numberdialog box, make the desired changes to the name or phone number.
- ClickOKto return to theDialer Configurationwindow. The expanded phone book displays the modified name or phone number.
Provide Feedback