Create a backup name or phone number
How do I access the dialog box?
To access the
Dialer Configuration
window, refer to the Configure a modem dialer topic.- From theDialer Configurationdialog box, expand the phone book that contains the name and phone number, for which you want to create a backup name or phone number.
- Select the desired entry from the phone book.
- SelectNew > Backup Phone Number.
- In theNew Backup Phone Numberdialog box, enter a name and phone number.
- ClickOKto return to theDialer Configurationdialog box. The expanded phone book shows the new backup name or phone number.
Provide Feedback