Change the modem's port configuration
How do I access this dialog box?
To access the
Dialer Configuration
dialog box, refer to the Configure a modem dialer help topic.- From theDialer Configurationdialog box, selectConfiguration > Port.
- Make the desired changes to the configuration parameters.
- After making the desired changes, clickOKto return to theDialer Configurationdialog box.
Provide Feedback