Add a name and phone number to an existing phone book
How do I access this dialog box?
To access the
Dialer Configuration
windows, refer to Configure a modem dialer.- From theDialer Configuration dialog box,select the phone book, to which you want to add a new name and phone number.
- SelectNew > Phone Number.
- Enter a new name and phone number to be included in the phone book.
- ClickOKto return to theDialer Configurationdialog box. The phone book is expanded to show the new name and phone number.
Provide Feedback