Set network browse addresses
To set network browse adresses, right-click a configured driver in
RSWho
and select Properties
.From the network properties sheet, enable Browse only the specified addresses to instruct RSLinx Classic to query only specific addresses. Enter a minimum/lowest address and maximum/highest address for RSLinx Classic to query. RSLinx Classic will query the range of address specified, inclusive, ignoring the Active Node Table (DH+/DH485), Max Node Address (DH485), or sMax/uMax (ControlNet).
Provide Feedback