Configure Gateway
The
Configure Gateway
menu option only appears when running the RSLinx Classic Gateway. It does not appear if you are running RSLinx Classic Lite, RSLinx Classic Single Node, RSLinx Classic OEM, or RSLinx Classic.The
General
tab on the Configure RSLinx Classic Gateway
dialog box contains a check box that allows you to enable the RSLinx Classic Gateway. When you choose to enable the RSLinx Classic Gateway, the changes will not take effect until you shut down and restart RSLinx Classic.Provide Feedback