Gateway Diagnostics
The Gateway Diagnostics menu option only appears when running the RSLinx Classic Gateway. It does not appear if you are running RSLinx Classic Lite, RSLinx Classic Single Node, RSLinx Classic OEM, or RSLinx Classic.
RSLinx Classic Gateway diagnostics are found under the General, Performance, Connection Event Log, and Active Connections tabs in the tabbed dialog.
Provide Feedback