Establish a RAS to the RSLinx Classic Gateway
- Ensure the RAS server is up and running RSLinx Classic Gateway.
- On the client machine, dial into the server.
- Open RSLinx Classic.
- SelectCommunication > Configure Drivers.
- From theAvailable Driverslist, selectRemote Device via RSLinx Classic Gatewayand clickAdd New.
- In the Server’s IP Address or hostname text box, enter the server's IP address and clickBrowseto show all the devices connected to the RAS server.
Provide Feedback