Compact harmony files in RSLinx Classic
RSLinx Classic
v3.90.00 (CPR 9 SR 9) allows you to compact existing harmony topology through the RSLinx Classic
user interface, instead of manually locating and deleting the harmony files from your computer's hard drive. This reduces the waiting time to open RSLinx Classic
, or to expand the driver nodes in the RSWho
.
IMPORTANT:
This operation deletes the browsed topologies and configured DDE/OPC topics in
RSLinx Classic
. If you are using RSLinx Classic
for OPC communications, RSLinx Classic
will not be able to serve data for the defined topics after the operation is completed. To re-establish communications after you have compact harmony files, you must re-open the application which uses
RSLinx Classic
, edit the topic in RSLinx Classic
, re-browse and select a target device for each topic within RSLinx Classic
's Topic Configuration.To compact harmony files:
- InRSLinx Classicmenu bar, clickFile > Compact Harmony,orInRSLinx ClassicLaunch Control Panel, clickTools > Compact Harmony.
- The following warning message shows. Read the message and clickYesto continue, or clickNoto cancel the compact harmony operation."This operation will delete all of theRSLinx Classicstored topology information. If you are usingRSLinx Classicfor OPC communications, after the Compact Harmony Database operation is completed,RSLinx Classicwill not be able to serve data for defined topics. To re-establish communications, you must manually browse and select a target device for each topic withinRSLinx Classic's Topic Configuration. Do you want to continue?"
- IfRSLinx Classicor the Harmony service is running, the following warning message shows. Read the message and clickYesto continue, or clickNoto cancel the compact harmony operation."RSLinx Classicand Harmony service need to be shut down in order to perform this operation. Shut downRSLinx Classicand Harmony services?"TIP:(Optional) Clear theRestart RSLinx Classic when finishedcheck box if you do not want to restartRSLinx Classicafter the compact harmony process. This option is selected by default.
- If the system detectsRSLinx Classicis in use by any other applications, the following warning message shows. Read the message and clickYesto continue, or clickNoto cancel the compact harmony operation."RSLinx Classicis currently in use by one or more applications. IfRSLinx Classicis shut down now, these applications will experience timeouts and/or loss of data. Shut downRSLinx Classicanyway?"
- Depending on your Windows User Account Control (UAC) level, an UAC warning message may show to confirm whether to make changes to your computer or not. ClickYesto start the compact harmony process.
- The progress begins and theCompact Harmony Progressdialog box shows with progress bar. ClickDetailto show or hide progress details.TIP:During the compact harmony process, theOKbutton is disabled. The button is enabled once the compact harmony progress is completed or failed.
- When the compact harmony process is completed, clickOK.
Provide Feedback