About FactoryTalk Security

FactoryTalk Security™ is intended to improve the security of your automation system by limiting access to those with a legitimate need. FactoryTalk Security authenticates user identities and authorizes user requests to access a FactoryTalk-enabled system. These security services are fully integrated into the FactoryTalk Directory and are included as part of the FactoryTalk Services Platform that installs with many products.
TIP:
If you did not use the default install paths while installing your Rockwell Software products, the preceding link will not work properly. Go to
x:\Program Files\Common Files\Rockwell\Help
to launch the FactoryTalk Security help file (FTSecurityEN.chm) manually (where
x:
is the drive where your Rockwell Software products are located).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal