Considerations when using RSLinx Classic with FactoryTalk Security
Keep the following in mind when using RSLinx Classic with FactoryTalk Security:
- Network/Local DirectoryThe FactoryTalk Services Platform can install two completely separate and independent FactoryTalk Directories: a Local Directory and a Network Directory. User accounts, passwords, and security permissions to securable features are completely separate and cannot be shared between the Network Directory and the Local Directory. Configuring any of these items on one directory does not configure them on the other. Similarly, changing the password to a user account in one directory does not change the password to the other directory, even if the account has the same name in both directories.When configuring RSLinx Classic to work in one of the two directories, please keep the following in mind:
- RSLinx Classic security policies and RSSecurity Emulator must be installed in the same directory (either Local or Network).
- If you configured RSLinx Classic to work in the Network Directory, you must use FactoryTalk Security to administer centralized security across the network.
- If you configured RSLinx Classic to work in the Local Directory and want to use FactoryTalk Security, you can administer security only on a single computer.
- Reset Network TreeWhen RSLinx Classic is reinstalled, all security settings that were previously configured for networks and devices are lost. You must redefine these security settings in the Networks and Devices tree, or in RSWho.If you did not select theEnable Securitycheck box during the RSLinx Classic installation, but want to enable security now, you need to modify the existing RSLinx Classic installation in Control Panel. Follow the steps below:
- SelectAdd or Remove ProgramsorPrograms and Featuresin the WindowsControl Panel. In the list of installed programs, right clickRSLinx Classic 3.73.00 CPR 9 SR 7.3, and then select Change. The RSLinx Classic Setup Wizard opens.
- While running the RSLinx Classic Setup Wizard, in theProgram Maintenancepage, selectModify.
- While running the RSLinx Classic Setup Wizard, in theRSLinx Classic Security Configuration Selectionpage, selectEnable Security.
- ClickNextto finish the RSLinx Classic installation changes.
- Every time you are in RSLinx Classic, be sure to verify that the username shown in theCurrent Security Usertext box of theSet Securitydialog box (Security > Set Security User) is correct. If it is incorrect, enter the new username and password, and clickOK.
Provide Feedback