Hardware DEP settings

Hardware DEP uses the processor to mark memory so that code cannot be executed from data regions. When code attempts to execute in these marked areas, the processor generates an exception. Hardware DEP is enabled as the factory default setting. This feature is turned on or off in the computer BIOS settings.
To determine if your hardware supports DEP, refer to the hardware manual or contact your hardware manufacturer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal